Search FAQs
How to do RTD input protocol settings in REL52812 (VIO 12AB)
By setting the REL52812 (VIO 12AB) module’s address to ‘0’, it is possible to send RTD measurements to the relay via the RTD input protocol
Note: When implementing the connection between REL52812 and a relay with RS-485 via the RTD input protocol, no other modules can be connected to the RS-485 bus.
Note: When implementing the connection between REL52812 and a relay with RS-485 via the RTD input protocol, no other modules can be connected to the RS-485 bus.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: