Search FAQs
Which LTMR or Tesys T base model is compatible with External Current Transformer
For motor having higher current rating greater than 100 Amp it is recommended to use external CT's of rating 100, 200, 400 and 800 amp and these external Current Transformer's are compatible with LTMR08*** model only.
For external CT's item code please check the document attached.
For external CT's item code please check the document attached.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: