{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to identify the CPU card in MiCOM C264 installed.
To identify the CPU card in a MiCOM C264.
One has to keep the complete Cortec of MiCOM C264.
For Example:   C264T21I6A1000240200B001111D00 

The 6 digit after C264 denotes the CPU card details in the C264 installed, for above-mentioned model the 6 Digit is "A"
A stands for CPU275 (Type 4) , with 2*Ethernet RJ45, 128Mb FlashMem, 256Mb SDRAM, 50 ppm Oscill (Ref CPU275 =2072282A01).

For further details, one has to go through the Order form of MiCOM C264. 

Schneider Electric India

Attachment(s)
C264 OrderForm_v04_072017.xlsm [262.84 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.