Search FAQs
Should we use fuses for the control power of meter.
You should include fuses at the control power terminals.
L1 and L2 are non-polarized. If using an AC power supply with neutral, connect neutral to the meter’s L2 terminal.
Always use a fuse on L1. Fuse L2 when connecting an ungrounded neutral to the control power. If using a control power transformer,
fuse both primary and secondary sides of the transformer. The fuses / circuit breakers must be rated for the installation voltage and sized
for the available fault current.
Kindly find the attachment for the instruction.
L1 and L2 are non-polarized. If using an AC power supply with neutral, connect neutral to the meter’s L2 terminal.
Always use a fuse on L1. Fuse L2 when connecting an ungrounded neutral to the control power. If using a control power transformer,
fuse both primary and secondary sides of the transformer. The fuses / circuit breakers must be rated for the installation voltage and sized
for the available fault current.
Kindly find the attachment for the instruction.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: