{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are control power characteristics of EM7200 series meters.

AC: 90-277 V L-N ±10%
DC: 125-250 V ± 20%
BURDEN: Auxiliary supply (control power): Max 10 VA at 240 Vac; Max 4.5 W at 300 Vdc

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: