{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the procedure for Primary current injection testing procedure for MCCB with TMD Trip unit
Please find attached document for stepwise explanation of  Primary current injection testing procedure for MCCB with TMD Trip unit. The test method method that MCCB can be tested with single phase as well as three phase. Single phase test results might not be the same as three phase testing together..

Note: TMD has its co-efficiency when test on ambient temperature different than 40 degree, and also when test is done on one pole For all the TMD curves, You may know that the catalogue tripping curves are given for an ambient temperature of 40°C in cold start condition and 3 poles loaded.
For 1 pole tripping, read the time corresponding to 0.85 times given current.
         

Schneider Electric India

Attachment(s)
Primary current injection testing procedure for TMD MCCBs.pdf [207.29 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.