{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is LCF( E60) fault on Altivar AFE (Active Front End).
Description: Error in the LFM, the control of the LFM or mains voltage missing.
Cause: The charging of the DC link has not been completed successfully because the required voltage level has not been reached.
Remedy: Check the DC link voltage and the charging resistors and fuses in the LFM. Furthermore, check whether the activation of the LFM corresponds with the circuit diagram.
 

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: