Search FAQs
How to read energy value on PM2100 displayed on front of LCD
Autoscaling is enabled for energy value in PM2100 meter.
Till 9999.9 meter displays in Wh units only. It changes to kWh after value reaches 9999.9 Wh.
When energy value reaches to 9999.9 Wh meter displays 10kWh.
For example, refer to the attachment showing energy reading.
The value showing on the display is 262407.382 kWh
Till 9999.9 meter displays in Wh units only. It changes to kWh after value reaches 9999.9 Wh.
When energy value reaches to 9999.9 Wh meter displays 10kWh.
For example, refer to the attachment showing energy reading.
The value showing on the display is 262407.382 kWh
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: