Search FAQs
How to Create, Modify and Delete password in Somove software
This function is available with the extended mode using SoMove, in the connected mode. It allows the
creation of a password to avoid modification of LTMR parameters by unauthorized people.
When a password is set, unauthorized users can view the displayed information, but cannot edit parameter values.
The password must be an integer from 0001 to 9999.
The password is also required to execute the SoMove Store to Device function.
For instruction kindly find attached document.
creation of a password to avoid modification of LTMR parameters by unauthorized people.
When a password is set, unauthorized users can view the displayed information, but cannot edit parameter values.
The password must be an integer from 0001 to 9999.
The password is also required to execute the SoMove Store to Device function.
For instruction kindly find attached document.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: