{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to backup the error log in Ecostruxure Machine Expert Basic.
SD card can be used to backup or delete the error log file of the logic controller.
Follow the below steps :
1. Create a file named script.cmd using notepad on your PC.
2. Add the following line in the file - Upload "/sys/log"
3. Copy the file to the root folder of the SD card.
4. Insert the SD card into the logic controller. Transfer of the error log file begins and the SD LED on the logic controller gets illuminated. Do not remove power during this operation.
5. After the operation, SD led is off or flashing.
6. The error log file PLClog.csv is saved on the SD card.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: