Search FAQs
HMI of P642 is no display,
Try to adjust LCD contrast but nothing changed at all.
it is display blank issue (Known issue). It is sufficient to load the model & serial number(Cortec) to relay to make it healthy. But kindly note it is suggested to load the same with E4 cable & software.
If you want the firmware we would be requiring the software subversion as well, that will be there in the Setting file which was extracted from the relay
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: