Search FAQs
Which toroids are recommended for Insulation Fault Locator
The toroids are used to connect the device to the channels of the system, which
can be monitored. The compatible toroids are
1) TA30
NOTE: This toroid is advised for IFL12H.
2) PA50
3) IA80
4) MA120
5) SA200
6) GA300
7) TOA80
8) TOA120
can be monitored. The compatible toroids are
1) TA30
NOTE: This toroid is advised for IFL12H.
2) PA50
3) IA80
4) MA120
5) SA200
6) GA300
7) TOA80
8) TOA120
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: