Search FAQs
What is the CT input specifications for the Varlogic VL series APFC relay
1 A/5 A nominal, 15 mA to 5 A (overload 6 A max, 10 s), 10 VA burden class 1 minimum.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: