Search FAQs
Will there be tools to take graphics from PLS 7.x, PSE 8.x and PSO 9.0 and automatically re-create those graphics in PSO 2020?
At the time of PSO 2020 release, we will not have tools to automatically re-create the 7.x, 8.x or 9.0 graphic layouts in PSO 2020. That said, we are re-creating all the 7.x, 8.x and 9.0 Power graphics that can be used by engineers to more quickly re-create screens. Additionally, during H1 2020 we were release tools to reduce the manual efforts of re-creating the 7.x, 8. and 9.0 graphic layouts in PSO 2020.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: