{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Maximum number of Inputs/Outputs ports available in Sepam 20 and Sepam 40 series.

The 4 outputs included on the Sepam series 20 and 40 base unit can be extended by
adding an optional MES114 module with 10 inputs and 4 outputs, available in 3
versions:

MES114: 10 DC inputs, the voltage from 24 V DC to 250 V DC
MES114E: 10 inputs, voltage 110-125 V AC or V DC
MES114F: 10 inputs, voltage 220-250 V AC or V DC

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: