As you can run only one Easergy Studio installation on your PC, you first need to remove an older version. The below process will retain the earlier installed data models.
- Use Windows® Control Panel to call the Easergy Studio setup wizard.
- Press ‘Yes’ when asked whether you want to remove the application and all pertaining features.
- Press ‘No’ when asked whether you want to remove the data models from your disk.
- The wizard will remove all programs of Easergy Studio.
- Close the wizard, close the Control Panel.
- Run the new Easergy Studio installation executable.
- Select all options as done for the installation before.
- Do not agree to launch the Data Model Manager.
Released for:Schneider Electric India