Search FAQs
What is default IP address of MC80 PLC?
The lower rotary switch is set to CLEAR IP to use the MAC-based default IP address.
The default IP address format is 10.10.x.x
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
The default IP address format is 10.10.x.x
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: