Search FAQs
What are the specific System words for MC80 PLC?
Please refer the attached document. BMX XCA USB 018
BMX XCA USB 045
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
BMX XCA USB 045
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: