Search FAQs
Which tools or software’s required to update firmware of MC80 PLC?
The MC80 PLC Firmware upgrade is done using Unity Loader or SGBackup tool. The MC80 PLC provides a fast and reliable firmware upgrade from the Unity Loader to PLC through USB connection or through Ethernet connection. BMX XCA USB 018
BMX XCA USB 045
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
BMX XCA USB 045
10.10: is a fixed value
x: The last two fields in the default IP address are composed of the decimal equivalents of the last two hexadecimal bytes in the MAC address.
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: