Search FAQs
Which MC80 PLC model compatible with the terminal blocks BMX FTB 28X0
The Discrete Input and Output (Discrete I/O) is a 24 Vdc function connected using a 28-pin terminal block (BMXFTB28x0). It is a positive logic function where the 8 input channels receive current from the sensors (sink) and the 12 output channels provide current to the pre-actuators (source).
The Discrete I/O function is available on the following PLC:
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20310
BMK C80 30310
BMK C80 20300
There are three types of 20-pin terminal blocks:
BMX FTB 2010 screw clamp terminal blocks
BMX FTB 2000 caged terminal blocks
BMX FTB 2020 spring terminal blocks
The Discrete I/O function is available on the following PLC:
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20310
BMK C80 30310
BMK C80 20300
There are three types of 20-pin terminal blocks:
BMX FTB 2010 screw clamp terminal blocks
BMX FTB 2000 caged terminal blocks
BMX FTB 2020 spring terminal blocks
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: