Search FAQs
What is the maximum frequency of HSC IO counting input BMK C80 20310
The MC80 PLC’s High Speed Counting Input and Output (HSC I/O) function is an equivalent function like M340 EHC0200, which is compatible with the Unity Pro software and operates up to 60 kHz.
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20310
BMK C80 30310
BMK C80 20300
There are three types of 20-pin terminal blocks:
BMX FTB 2010 screw clamp terminal blocks
BMX FTB 2000 caged terminal blocks
BMX FTB 2020 spring terminal blocks
BMK C80 20301
BMK C80 30311
There are two types of 28-pin terminal blocks:
BMX FTB 2820 spring terminal blocks
BMX FTB 2800 caged terminal blocks
BMK C80 20310
BMK C80 30310
BMK C80 20300
There are three types of 20-pin terminal blocks:
BMX FTB 2010 screw clamp terminal blocks
BMX FTB 2000 caged terminal blocks
BMX FTB 2020 spring terminal blocks
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: