BOOL type, which contains only the value FALSE (=0) or TRUE (=1).
EBOOL type, which contains the value FALSE (=0) or TRUE (=1) but also information concerning the management of falling or rising edges and forcing.
Both EBOOL and BOOL are managed by Byte. The structure of EBOOL and BOOL is as follows:
BOOL:
EBOOL:
As EBOOL has forcing bit, we can force EBOOL variables but not BOOL variables.
For more information on this refer the attached document.
EBOOL type, which contains the value FALSE (=0) or TRUE (=1) but also information concerning the management of falling or rising edges and forcing.
Both EBOOL and BOOL are managed by Byte. The structure of EBOOL and BOOL is as follows:
BOOL:
7
|
6
|
5
|
4
|
3
|
2
|
1
|
0
|
|
|
|
|
|
|
|
Current Value
|
EBOOL:
7
|
6
|
5
|
4
|
3
|
2
|
1
|
0
|
|
|
|
|
|
Forcing Bit
|
Previous Value
|
Current Valur
|
As EBOOL has forcing bit, we can force EBOOL variables but not BOOL variables.
For more information on this refer the attached document.
Released for:Schneider Electric India