Steps for troubleshooting humming noise in ATV320:
- Check the noise reduction parameter 'nrd'. Try setting it to Yes and check.
- Check the parameter Switch Freq Type 'SFt'. Try setting it to HF2 and check.
If these settings does not resolve then check the below points in the installation site:
- Ensure all components are grounded appropriately.
- Using a shielded power cable to connect the variable frequency drive to the motor and correctly connecting the shield to drive and motor ground locations.
- Using motor Choke. If the cables are longer than 50 meter between drive and motor. Check the switching frequency and motor cable length.
- Using twisted control wiring leads to provide a balanced capacitive coupling.
- Running power and control wiring separately.
Released for:Schneider Electric India