undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to over come with Error "Please download runtime system from the editor" on Pro-Face HMI.

Force transfer of runtime file has to be performed via GP Pro-Ex.

Below steps can be under taken to perform this action.

Forcing the transfer of project files

If a project file cannot be transferred, you can force the display unit into transfer mode (waiting to receive project).

There are two ways to enter forced transfer mode:

  • Forced transfer by touching the screen
  • Forced transfer by setting DIP switches

Forced transfer by touching the screen

Using screen touch, you can forcibly transfer a project file.

For the GP-4000 and LT-4000 series, you can also run forced transfer using external storage.

*For models other than the GP-4000 and LT-4000 series

Using screen touch, you can forcibly transfer project files from GP-Pro EX.

1. When the power is turned on, continue touching the bottom left corner or the bottom right corner of the panel (within a 40 pixel area).

image1

2. When the following dialog box appears, transfer project files from GP-Pro EX.

After transfer is complete, the display unit restarts and the transferred project's initial screen is displayed.

Image2


*For GP-4000 and LT-4000 series

Using screen touch, you can forcibly transfer project files from GP-Pro EX.

1. When the power is turned on, continue touching the bottom left corner or the bottom right corner of the panel (within a 40 pixel area).

Image3

Image11 When using the GP-4100 series, continue touching the bottom left corner or bottom right corner (within 20 pixels of the edges) of the panel.

2. When the following dialog box appears, transfer project files from GP-Pro EX.

Image4


*When using external storage for the GP-4000 and LT-4000 series

In addition to transferring from GP-Pro EX, forced transfer is possible using external storage.

For forced transfer using external storage, from the [Memory Loader]'s [Transfer Tool] command, select [Create Backup File].

For the procedure on how to create backup data, see the following section.

Image12 Transfer - Transferring Project Files from PC to Display Unit

1. When the power is turned on, continue touching the bottom left corner or the bottom right corner of the panel (within a 40 pixel area).

Image5

Image13 When using the GP-4100 series, continue touching the bottom left corner or bottom right corner (within 20 pixels of the edge) of the panel.

2. When the following dialog box appears, touch [SD] or {USB].

Image6

3. This will restart the display unit and launch the Memory Loader tool. Touch [Download] on the following screen.

Image7

4. Select the file you want to transfer and touch [Start]. (If there is a password for transferring, input the password first, then touch [Start].)

Image8

5. After transfer is complete, the display unit restarts and the screen of the transferred project file is displayed.

*Forced transfer by setting DIP switches

Set DIP switch 2 to ON to force the transfer of the project file. When using a model without DIP switches (such as the GP-3302B), use forced transfer by touching the screen.

1. Ensure that the display unit is turned OFF and then open the CF card cover at the bottom. Locate the CF card interface and DIP switches inside the cover and set DIP switch 2 to the ON position.

Image9

2. When the GP is turned ON and the following dialog box appears, transfer the project file from the GP-Pro EX. After forced transfer is complete, the display unit restarts and returns to the force transfer screen.

Image10

3. Turn OFF the display unit and then set DIP switch 2 to OFF. When you turn ON the display unit again, the above screen is displayed. Touch the [Reset] button. Always use the display unit with DIP switch 2 set to OFF except when forcing the transfer of project files.

Above mentioned steps for Compulsion Transfer mode are also available in link below.

https://www.hmisource.com/otasuke/files/manual/gpproex/v3_12/refer/mergedProjects/maintenance/maintenance_pr_forced_transfer.htm

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: