{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
UPS BVX900LI-IN showing red led with constant tone ?
Possible Cause:  Occurrence of an overload condition.
Solution:1)The power being used by the connected equipment has exceeded the capacity of the unit.
2)Unplug devices connected to UPS output socket one at a time to remove overload.
Note: If the detected problem is not corrected, contact Schneider Electric customer care.

Schneider Electric India

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: