{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
UPS BVX900LI-IN is not any giving backup ?
Possible cause: Battery completely drained/ Battery ended its service life.
Solution:
1. Check how old is the unit, as the battery age/consumption increases battery backup time decreases.
2. Check whether UPS drops the load instantaneously as soon as the power fails.
3. Check the battery connection on the rear panel.
4. Check for the details on the recent power failure.
5. Did the UPS get sufficient time to charge the battery for 6 to 8hrs since the recent power outage.
6.Connect Easy UPS  to AC power for ten hours while the battery charges to full capacity.
If the detected problem is not corrected, contact Schneider Electric customer care.

Schneider Electric India

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: