{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Where can I found compatibility between Control Expert Versions, Application Versions and PLC OS for quantum plc.
Overview

Application version corresponds to the processor OS version displayed in Control Expert configuration screen.
The OS version corresponds to the minimum version required to execute an application functional level.
Higher OS versions provide compatibility with a lower application version.
For example, a Quantum application version V2.00 generated by Unity Pro V3.0 can be executed by a PLC OS version V2.40.
NOTE: Unity Pro is the former name of Control Expert for version 13.1 or earlier.
Modicon Premium Platform

This table gives the application version created with the different Control Expert/Unity Pro versions:

Modicon Quantum Platform

This table gives the application version created with the different Control Expert/Unity Pro versions:
Mininum OS versionUnity Pro / Control Expert
V2.0V2.1V2.2V2.3 SP1V3.0V3.1V4.0V4.1V5.0V6.0V6.1V7.0V8.0V8.1V10.0...V15.0
140 CPU 311 102.002.302.602.803.003.20
140 CPU 434 12A/U2.002.302.602.803.003.20
140 CPU 534 14A/B/U2.002.302.602.803.003.20
140 CPU 651 50NA2.302.602.803.003.103.203.30
140 CPU 651 602.002.302.602.803.003.103.203.30
140 CPU 652 60NA2.402.602.803.003.103.203.30
140 CPU 658 60NA3.203.30
140 CPU 670 60NA3.103.203.30
140 CPU 671 602.002.302.602.803.003.103.203.30
140 CPU 672 60NA3.103.203.30
140 CPU 672 61NA2.803.003.103.203.30
140 CPU 678 61NA3.203.30

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.