{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to Force CamSwitch Configured Digital Output manually in PacDrive?

We can't force the output on the CamSwitchGroup,

but you should be able to realize the request by adding a piece of logic to the code.

The idea is to set no 'Destination' on the CSG, only use the output 'Value' of the CSG.

Then you can connect this signal with other signals (f.e. from HMI) and transfer the result to the digital output.

pacdrive

Schneider Electric India