Search FAQs
Video: How to do the PTO configuration in M241 PLC
This video demonstrates how to do the PTO configuration in M241 PLC , EcoStruxure Machine Expert is used for programming TM2XX logic controller and Motion Controller.
this video helps you on how to generate pulse train output through M241 PLC and used for different servo drives.
EcoStruxure Machine Expert can be used for programming of TM241 , TM251 Logic controllers and TM262 Motion controller. Pulse train output are used for basic motion application
where in the servo drive run with the help of pulse generated from PLC.
this video helps you on how to generate pulse train output through M241 PLC and used for different servo drives.
EcoStruxure Machine Expert can be used for programming of TM241 , TM251 Logic controllers and TM262 Motion controller. Pulse train output are used for basic motion application
where in the servo drive run with the help of pulse generated from PLC.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: