{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is BMCXM0100 module compatible with BMXXBPxxxx rack

The BMECXM module will only power up on a BMEXBP•••• Ethernet backplane.

Selecting a Backplane

On the BMEXBP•••• backplanes, the BMECXM module can be mounted in any open slot, except
the following restrictions:
> When mounted on a local rack, slots 0 and 1 are reserved for the M580 CPU.
> When mounted on a remote drop, slot 0 is reserved for the drop end communicator module.
In addition to the above restrictions on BMEXBP•••• backplanes, some open slots are not allowed

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: