What is Rated short-time withstand current: Ik (A)?
This is the rms value of the current which the switchgear can carry in the closed position during a specified short time. Short time is generally 1 s, and sometimes 3 s.
Released for:Schneider Electric India
Explore more
Range:
MCSet 17.5 kV
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.