Can we use remote indication in CVS/ EZC MCCB with help of SD or SDTAM modules?
SDx and SDTAM are relay modules with two static outputs. They send different signals depending on the type of fault. They may not be used together. They cannot be used with CVS/EZC MCCB.
Released for:Schneider Electric India
Explore more
Range:
EasyPact CVS
EasyPact EZC
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.