{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I access devices in a M580 Ethernet IO network via the SERVICE port (ETH1) when it is configured in port mirror mode.

SERVICE port (ETH1) can be configured either as a “Access Mode” or “Port mirror Mode”.

When the SERVICE port is configured in access mode, then you can access devices in a M580 network via any tool.
When the SERVICE port is configured in port mirror mode, you cannot access devices — that is, you cannot ping other devices
by connecting a PC to ETH1 in port mirror mode.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: