{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the default password of the Easergy P3 relay?
By default, the Easergy P3 device has five user accounts.
User accountUser nameDefault passwordUse
Useruser0Used for reading parameter values, measurements, and events, for example
Operatoroperator1Used for controlling objects and for changing the protection stages’ settings, for example
Configuratorconf2Needed during the device commissioning. For example, the scaling of the voltage and current transformers can be set only with this user account. Also used for logging on to the HTTP server
Administratoradmin3Needed for changing the passwords for other user accounts and for creating new user accounts
Easergyeasergy2Used for logging on to the FTP server

Schneider Electric India

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: