Search FAQs
How to switch command channel from Cd1 to Cd2 in ATV320?
Please refer to the below settings to enter the parameter CCS (Cmd Switching)
DRI- > CONF > FULL > CTL
This parameter can be accessed if [Profile] (CHCF) is set to [Separate] (SEP) or [I/O profile] (IO).
For Command channel switching you can configure LI1 to LI6.
If the assigned input or bit is at 0, channel [Cmd channel 1] (Cd1) is active.
If the assigned input or bit is at 1, channel [Cmd channel 2] (Cd2) is active.
If [Profile] (CHCF) is set to [Not separ.] (SIM), only [Cmd channel 1] (Cd1) setting value is possible.
[ch1 active] (Cd1): [Cmd channel 1] (Cd1) active (no switching)
[ch2 active] (Cd2): [Cmd channel 2] (Cd2) active (no switching)
[LIx] (LI1): Logical input LI1....LI6
DRI- > CONF > FULL > CTL
This parameter can be accessed if [Profile] (CHCF) is set to [Separate] (SEP) or [I/O profile] (IO).
For Command channel switching you can configure LI1 to LI6.
If the assigned input or bit is at 0, channel [Cmd channel 1] (Cd1) is active.
If the assigned input or bit is at 1, channel [Cmd channel 2] (Cd2) is active.
If [Profile] (CHCF) is set to [Not separ.] (SIM), only [Cmd channel 1] (Cd1) setting value is possible.
[ch1 active] (Cd1): [Cmd channel 1] (Cd1) active (no switching)
[ch2 active] (Cd2): [Cmd channel 2] (Cd2) active (no switching)
[LIx] (LI1): Logical input LI1....LI6
Released for:Schneider Electric India
Explore more
Product:
Explore more
Product: