Search FAQs
What is the system requirements to install Advantys 12.3.0.0?
Below are the hardware requirements for using Advantys 12.3.0.0.
This table describes the minimum hardware requirements to run the Advantys Configuration Software on Microsoft Windows 7 Professional (32/64 bits), Windows 8 Pro (64 bits), Windows 8.1 (32/64 bits), Windows 10, Windows Server 2008 R2 (64 bits), and Windows Server 2012 R2 (64 bits):
This table describes the minimum hardware requirements to run the Advantys Configuration Software on Microsoft Windows XP Professional:
A CD-ROM drive is the required installation medium.
Virtual Machine
The Advantys Configuration Software runs on the following virtual machines:
This table describes the minimum hardware requirements to run the Advantys Configuration Software on Microsoft Windows 7 Professional (32/64 bits), Windows 8 Pro (64 bits), Windows 8.1 (32/64 bits), Windows 10, Windows Server 2008 R2 (64 bits), and Windows Server 2012 R2 (64 bits):
Requirement | Minimum |
---|---|
System | Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz |
RAM | 2 GB, recommended 3 GB |
Hard Disk | Minimum available free space 2 GB, recommended 10 GB |
Microsoft Internet Explorer 5.5 or higher |
This table describes the minimum hardware requirements to run the Advantys Configuration Software on Microsoft Windows XP Professional:
Requirement | Minimum |
---|---|
System | Pentium Processor 1.2 GHz or higher, recommended 3.0 GHz |
RAM | 1 GB, recommended 2 GB |
Hard Disk | Minimum available free space 2 GB, recommended 5 GB |
Microsoft Internet Explorer 5.5 or higher |
A CD-ROM drive is the required installation medium.
Virtual Machine
The Advantys Configuration Software runs on the following virtual machines:
- VirtualBox
- VMWare
Released for:Schneider Electric India
Explore more
Product:
Explore more
Product: