{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are pollution degree & degree of protection of ATV320?
Drive                               Pollution Degree                         Degree of Protection

ATV320.....B                                2                                              IP20
ATV320.....C                                2                                              IP20
ATV320.....W                               3                                              IP66
UL Type 4X Indoor(1)
ATV320.....WS                             3                                              IP65
UL Type 12

(1): ATV320•••••W drives can get UL Type 4X Indoor rating, when fitted with the following option kits:
 VW3A9923X for ATV320U••M2W and ATV320U04...U40N4W,
 VW3A9924X for ATV320U55N4W and ATV320U75N4W.

Schneider Electric India

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: