{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What do if there is "HOT" error code on display for Easy UPS SRV2KUXI-IN ?
Probable cause:

The temperature of the unit is rising above the set limits.

Possible Solution:

1. Disconnect non-essential equipment from the Easy-UPS to reduce the Easy-UPS load.
2. Maintain operating temperature between 0° to 40°C at full load and 40° to 50°C linearly derated to 75% of the load.
3. Do not operate UPS where there is excessive dust or where the temperature or humidity is outside specified limits.
4. Do manual restart of UPS by switching off the output, turning off the input power supply, and turning On the input and output, this should resolve the issue

In case the error persists even after trying the above troubleshooting, log the complaint.

Schneider Electric India

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: