{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where can I get the 3D CAD drawing for ABL6 transformer ABL6TS100U?

This ABL6 transformer supplies alternating current to control circuits while isolating them from mains power. It has a rated input voltage of 230V to 400V AC, a rated output voltage of 230V AC and a rated power of 1kVA / 1000VA. It offers an economic way to supply each consuming load individually, or by groups of loads, in applications such as mining, refining. It is ideal for systems accepting low voltage AC power, such as motor protection relays, contactors.

Check the attach file for 3D CAD file.

Schneider Electric India

Attachment(s)

MCADID0005657_3D-CAD.zipMCADID0005657_3D-CAD.zip [876.97 KB]
Explore more
Product:
ABL6TS100U
Explore more
Product:
ABL6TS100U
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.