{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the system requirements to use Control Expert v15.2.
Minimum and recommended computer configuration
The following table describes the system requirements to install and use Control Expert.
 
Minimum and recommended computer configuration
CPU2.4 GHz. 3.0 GHz or higher recommended.
Core i3 or higher. Core i7 or higher recommended.
RAM8 GB. 16 GB recommended
16 GB minimum for Windows Server
Storage8 GB including the space for the software installation, execution, and for saving applications. 20 GB  recommended.
SSD drive are recommended
Operating system and versionMicrosoft Windows 10 64-bit, version 21H1 or newer
Microsoft Windows 10 64-bit Enterprise 2019 LTSC, version 1809
Microsoft Windows Server 2019, standard 1809 version
DriveDVD R to install the software. DVD RW recommended.
DisplayVGA (800 x 600) minimum resolution.
Maximum recommended resolution 2560 x 1440 with Scale and Layout at 125%.
Input devicesKeyboard and mouse or compatible pointing device.
Web accessLicense activation on the Internet is recommended.
Offline activation remains possible (please refer to License Manager or Floating License Manager)
OtherUSB port
Note: Windows 10 32-bit is not supported.
 
EcoStruxure Control Expert V15.2 has been tested with the following antivirus/protection active:
1. McAfee Virus Scan Entreprise V8.8
2.Cylance Protect 2.0.1534.15 (Windows 10)
3.Defender for Windows 10
 
Control Expert requires Microsoft .NET 3.5 SP1
Depending on the target Windows version and Windows configuration, .Net versions may be:
 1. Not installed
 2. Installed but not enabled (the related "windows feature"  is not set ON)
 3. Installed and enabled
 
Control Expert setup automatically tries to install and enable the required .Net Framework on the target Windows if necessary.
 
On Windows 10 and Windows Server 2019, automatic or manual installation of .Net Framework 3.5 requires an internet connection.
And  the “Windows Update” service must be started in order to install the .NET Framework 3.5.
 
.NET Framework 3.5 SP1can be downloaded from
https://dotnet.microsoft.com/download/dotnet-framework/net35-sp1
 Select: Download .NET Framework 3.5 SP1 Runtime
 
Control Expert requires Microsoft .NET Framework 4.8
.NET Framework 4.8 is natively installed on Windows 10 version 1903 and after.
.NET Framework 4.8 can be downloaded from
https://dotnet.microsoft.com/download/dotnet-framework/net48
Go to “Advanced downloads”, select Offline installer: Runtime

Virtualization
Control Expert V15.2 has been successfully tested in the following configuration:
·        VMware vSphere –Hypervisor- ESXi
·        VMware Workstation 15.5.2
·        Oracle VirtualBox 6.1.0
Note: It has not been tested on Virtual Box 5.2.16-123759
Note: The amount of RAM of host computer needs to be 16 GB if Control Expert is used in a Virtual machine with 8 GB assigned to the Virtual machine.
 

Schneider Electric India

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.