I bit della Drivecom state register [ETA] o status word hanno il seguente significato:
Possible values in CiA402 profile, separate or not separate mode:
Bit 0 = 1: "Ready to switch on", awaiting power section line supply
Bit 1 = 1: "Switched on", ready
Bit 2 = 1: "Operation enabled", running
Bit 3 = 1: Fault detection
Bit 4 "Voltage enabled", power part connected to supply mains
= 0: Power part not connected to supply mains
= 1: Power part connected to supply mains
When the drive is powered by the power section only, this bit is always at 1.
Bit 5 Bit 5: = 0: Quick stop
Bit 6 Bit 6: = 1: "Switched on disabled", power section line supply locked
Bit 7 Bit 7: Warning
= 0: No warning
= 1: Warning active
Bit 8 Bit 8: Reserved (= 0)
Bit 9 Bit 9: Remote: command or reference via fieldbus
= 0: Command or reference given via the graphic display terminal or remote display terminal
= 1: Command or reference via fieldbus
Bit 10 Bit 10: Target reference reached
= 0: The reference is not reached
= 1: The reference has been reached
When the drive is in speed mode, this is the reference frequency.
Bit 11 Bit 11: "Internal limit active", reference outside limits
= 0: The reference is within the limits
= 1: The reference is not within the limits
When the drive is in speed mode, the limits are defined by the [Low speed] (LSP) and [High speed] (HSP) parameters.
Bit 12 Bit 12: Reserved (= 0)
Bit 13 Bit 13: Reserved (= 0)
Bit 14 Bit 14: "Stop key", STOP via stop key
= 0: STOP key not active
= 1: Stop triggered by the STOP key on the graphic display terminal or the remote display terminal
Bit 15 Bit 15: "Direction", direction of rotation
= 0: Forward rotation at output
= 1: Reverse rotation at output
The combination of Bits 0, 1, 2, 4, 5 and 6 defines the state in the DSP 402 state chart (refer to fieldbus manuals).
Pubblicato per:Schneider Electric Italy