Issue:
Wondering if the ATS48 comes with the shorting contactor, as a standard component when it is ordered?
Product Line:
ATS48
Environment:
Shorting contactor
Cause:
n/a
Resolution:
No. It can be ordered as a separate component to be added in the field.
Wondering if the ATS48 comes with the shorting contactor, as a standard component when it is ordered?
Product Line:
ATS48
Environment:
Shorting contactor
Cause:
n/a
Resolution:
No. It can be ordered as a separate component to be added in the field.
게시 대상:슈나이더 일렉트릭 Korea