Issue:
Causes of an IFI fault on the ATV312 drive
Product Line:
Altivar, ATV312
Environment:
All
Cause:
Unknown rating
Resolution:
Try power cycling the drive to see if the IFI fault clears. If it does not clear, replace the drive.
Reference manual BBV46385
게시 대상:슈나이더 일렉트릭 Korea