{}

브랜드

Impact-Company-Logo-English Black-01-177x54

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.

FAQ 검색

What is the basic ATV12 Modbus setup?

Issue:
ATV12 Modbus set up.

Product Line:
Altivar ATV12

Environment:
All

Cause:
Needs Modbus setup assistance.

Resolution:
Goto:
Conf enter
Full enter
CON enter

ADD= Modbus address 1 thru 127
Tbr= network speed baud rate 19.2
tFO= Format 8E1
trO= Timeout 10 seconds

Writing speed in RPM’s
CMD word is 8601 is the start and stop
LFRD speed set point 8602 is Frequency reference in RPM’s

Writing speed in HZ’s
CMD word is 8501 is the start and stop
LFRD speed set point 8502 is Frequency reference in HZ

Reading drive status and output speed
ETA Status Word 8603 monitoring motor speed in RPMs
ETS Status Word 8501 monitoring motor speed in HZ

To start the drive you write a Decimal value 6,  then 7 then 15 to word 8601 or 8501  (Check for offset in Server  controller)
Speed Freq  in HZ, Write value to 8502. Speed in RPM, Write value to 8602.
The Modbus Registers are 4X or 40X Holding registers.

슈나이더 일렉트릭 Korea

첨부 파일

Setting up the ATV12 for Modbus control.pdfSetting up the ATV12 for Modbus control.pdf [85.28 KB]
자세히 알아보기
제품군
Altivar 12
자세히 알아보기
제품군
Altivar 12