Issue:
How to add a Quantum NOM module into the local rack with Concept software.
Product Line:
Quantum, Concept
Resolution:
To add a NOM module into the local rack first open the I/O Map and choose "Head Setup".
Under NOM in the Head Setup change the Link 1 slot number to the slot number that the NOM will be installed
Now Go into the Local Drop in the I/O map and the NOM will show up in the Slot number chosen
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
게시 대상:슈나이더 일렉트릭 Korea