Issue
The purpose of this Resolution is to inform Advantys users of changes in the I/O modules current consumption specifications.
Some of the publications have incorrect 5.25v backplane current consumption values specified.
Product Line
Advantys STB
Environment
Resolution
The following documents are affected:
- The online Help in Advantys Configuration Software versions 1.2 or less.
- The Advantys STB Hardware Components Reference Guide, 890USE17200, version 3.0 and less.
The Resource Analysis option in Advantys Configuration Software version 1.2 contains the correct values.
The attached document lists the Advantys modules and the current that is either supplied or consumed by the device.
Attachments
Advantys_Module_power10-8-04.doc