Issue
The purpose of this resolution is to inform Advantys STB users of restrictions regarding FTX ES 00 software.
Product Line
The FTX ES 00 is free software that does not require registration. It contains the OTB/FTM software and
the STB Lite version configuration software.
STB Lite software is a demonstration version. If using it, you cannot go online, nor download. It cannot be
converted to a full version by merely transferring registration. You need to install the full version before attempting
an authorization transfer.
Resolution
Reference the attached document for information on how FTX ES 00 and STBSPU1000 can coexist in the same PC.
Legacy KB System (APS) Data: RESL170483 V3.0, Originally authored by on , Last Edited by on
Related ranges: Advantys STB
게시 대상:슈나이더 일렉트릭 Korea