Issue
What are the physical dimension specifications for the single slot Quantum modules?
Product line
Modicon Quantum
Environment
140CPU67261
Resolution
The dimensions for the single slot Quantum modules are:
Height = 9.84 in. (250 mm)
Depth = 4.09 in. (103.85 mm)
Width = 1.59 in. (40.34 mm)
게시 대상:슈나이더 일렉트릭 Korea