Issue
The purpose of this resolution is to suggest corrective actions which may be taken in the event error indications are displayed in the Ethernet NIM Diagnostic registers.
Product Line
Advantys, STB
Resolution
Reference the attachment Diagnostic Data Corrective Actions for recommendations in the event errors are displayed in the STBNIP2212 Ethernet NIM Diagnostic registers. A description of the registers may be found in the Advantys STB Ethernet Modbus TCP\IP Network Interface Applications Guide, p/n 890USE17700, Data Exchange Chapter 6, Reading Diagnostic Data.
게시 대상:슈나이더 일렉트릭 Korea