Issue
The purpose of this resolution is to inform 170ENT11001 Ethernet Communication Adapter users that the Web page files have been upgraded to v. 1.01.
The 170ENT11001 'Momentum I/O Values' web page does not display the data and module identity for the 170ADO83030 or 170AMM11030 I/O bases.
Product Line
Momentum
170ENT11000
170ADO83030
170AMM11030
Environment
Resolution
This resolution affects all 170ENT11001 Ethernet Communication Adapters with Web version less than 1.01.
Upgrading the web pages to version 1.01 will correct the web page display issue for the 170ADO83030 and 170AMM11030 modules.
The Web Page Download Procedure details the steps required to install web version 1.01.
Web files v.1.01 contains the files required to update the 170ENT11001 web pages.
Attachments:
Web Page Download Procedure
Web files v.1.01
게시 대상:슈나이더 일렉트릭 Korea